This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Through which bus temperature data are communicated ?

Part Number: AWR2243


Dear TI team,

We're testing our own radar design made of 4 AWR2243P in cascade mode.

We have a back-end hardward and application (validated on the devkit) that has CSI2 and SPI connections with each of the AWR2243P chip.

We expect to receive temperature data but it's not working so far (the back-end application can't provide temperature informations).

Hence my question : which bus (CSI2, SPI) is used by the AWR2243 chips to communicate their temperature data ?

Thanks

Charles