Other Parts Discussed in Thread: FDC2214,
Hello,
I've connected the FDC2214 in the following way, with the measurement capacitor in parallel and tested various caps measuring the resonance frequency with an oscilloscope between GND and IN0A or IN0B. I'm also able to read out the chip through I2C over a range from 70pF to about 200nF.

So far the measurements have been succesful but only up to capacitors around 8nF. Attached capacitors from 80nF and above only show disturbance on the oscilloscope measurement.
I'm using a RTB2002 scope with probes with a capacitance of 12pF and 10MOhm.
Its a bit confusing to me that it does work for the lower caps/higher frequencies, but not for the higher caps/lower frequencies.
Can someone explain this to me?