This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE3010: AFE3010 can meet CCID20(UL2231-2)

Part Number: AFE3010

Hi, Support Team

about AFE3010 can meet CCID20 (UL2231-2) requirements? Is this IC suitable for charging pile application?

if any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence

  • Hello Lawrence,

    I am no expert on the regulations of the UL2231-2 requirements. I believe they have many similarities to the UL943, which AFE3010 is compliant with.

    I can say that whatever UL2231-2 requirements that are the same as UL943, that AFE3010 can satisfy these.

    The AFE3010 can always be configured to trip at different thresholds or operate of higher line voltages. 

    Does this application require operating off a dual line? 

    Does the ground fault protection need to remain if one of the line voltages becomes inoperable?

    Sincerely,

    Peter

  • Hello Lawrence,

    I will close out this thread and mark as resolved assuming you have no more questions; however, if you do have any more questions please do not hesitate to ask them here or create a new thread.

    Sincerely,

    Peter