Other Parts Discussed in Thread: TDC1000
HELLO ~ ISSAC :
It has a long time not to consult the TDC1000 with you , here it is glad for me to thanks for your help and support before.
there is still one question to consult with you.
we utilize a water container with acrylic material and the bottom thickness is about 30 mm ( it is thicker than gereral one,and we know it is not a correct design) , we detect the height of water from the bottom and hence the sound wave goes through the 30 mm bottom thickness , the sound wave TOF is also calculated .
The question is that the TOF of bottom thickness ( acrylic material ) is included ?? or it could be ignored ? we know the sound speed of solid material is faster than clean water , however the TOF of bottom thickness could be ignored ?
thanks for your help~