This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: POE Powered (+48V)

Part Number: IWR6843
Other Parts Discussed in Thread: LMR38020, TPS7A92, LP87745-Q1

Dear E2E Support-

I am working on an IWR6843 radar design that uses 48V POE non-isolated power. I am trying to find the best power supply solution.

My current best solution is 48V -> LMR38020 switcher -> 3.4V -> TPS7A92 low-noise LDO -> 3.0V -> LP87745-Q1 triple buck (1.8V, 1.2V, 1.0V).

Do you have any recommendations or changes to this approach?

Thanks-

Mike Schell