This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004: FDC1004 suitable for capacitive force transducer design ?

Part Number: FDC1004
Other Parts Discussed in Thread: LDC1612, LDC1312,

Hi there,

I was thinking to use the FDC1004 in single ended configuration with shielding to measure a force applied to a heavy duty threat rod measuring the change in distance between two metal washers. The distance between the plates would be anything around 10mm. Reading to all datasheet and sample application I got the impression that the FDC1004 is too sensitive for this setup. Correct?

Best wishes