Other Parts Discussed in Thread: OPT3101
Hi Team,
Requirement: calibrate multiple tof at the same time.
The customer would like to know will there be any interference with each other when phase calibration is performed on multiple tof at the same time? For example, if tof No.1 is transmitting and receiving (when tof No.2 is working), would placing tof No. 2 in any space position (without occlusion No. 1 of) interfere with Tof No. 1 operation? And why?
Could you help check this case? Thanks.
Best Regards,
Cherry