This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Problems with Angle Estimation Using Virtual Antennas

Part Number: IWR6843AOPEVM


Hello,

May I ask if the 180° phase problem in the red part mentioned here will affect my angle estimation? I use the TDM-MIMO mode to obtain the data. Now I want to use 4, 3, 12, and 11 in the virtual array for FFT processing. To obtain an estimate of the pitch angle, will the phase difference of the red part shown in the figure affect my angle estimation, or if I want to use the data of this virtual array, I must first change all the phases of the red part before proceeding to subsequent angles estimate?

Regards,

Gary