Hi Team,
1) If the CFAR_out_mode parameter register is set to 10 or 11 (detect Peak List Mode), it will only output information about the detected peak target, but it is not clear that there are several peak targets before running. In this case, could you help share how to set up the DSTANCT, DSTAINDX, and DSTBIDNX in the output formatter?
2) And regarding the manual, it also describes the FFTPEAKCNT register, which indicates the number of peak targets to be taken by the host processor. Is this register counting the sum of multiple iterations of the currently running parameter set peak target or the peak target of one iteration (iteration: Reg_BCNT)?
--In the latter case, the current parameter set is not running and the number of peak targets for the second iteration will overwrite the number of peak targets for the first iteration, right?
--If the former is true, is it possible to continuously store multiple iterations of peak samples to target memory (MEM_2,3) if the output formatter is used, in the case of uncertainty about the number of peak targets (set parameter register)?
Could you please help check this case? Thanks.
Best Regards,
Cherry