Other Parts Discussed in Thread: IWR1843, UNIFLASH
Hi,
maybe hardware failure?
All working OK, developing & debugging in CCS 11 (update to 12 ... same error). Suddenly get this error:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 9.6.0.00172)
XDS110 ports X2 appear in device manager, mmwStudio works fine (recently re-installed to fix problem loading DCA1000, but CCS was OK after this), uniFlash7 OK - ccsdebug download.
So - tools seem happy & working, except CCS. Any suggestions of what to look at next?
many thanks
Alan Milne