Other Parts Discussed in Thread: IWR1642
HI.
Test cases in MMWAVE_L_SDK_05_03_00_02\examples\drivers\watchdog\watchdog_reset\xwrL64xx-evm\m4fss0-0_freertos. After triggering the watchdog timeout, the radar stopped printing output, and the radar did not respond, nor did it re-run the program. This is the same as the soft reset symptom. When using the watchdog_interrupt test case, what do I do in the callback function to trigger a watchdog reset?