Other Parts Discussed in Thread: FDC1004, FDC1004EVM
Hello,
I want to write my own PC program instead use the TI program "Sensing Solutions EVM GUI". I can get the channel values via comport with the command "1". It is also possible to set the any R/W register via comport or it is only with i2c possible? The programm "Sensing Solutions EVM GUI" can also set the register via comport. How is the command?
best regards
Güney Can