Hi experts,
I am testing the performance of the AWRL1432 development board.
The configured maximum range is about 85 meters. The configuration parameters are as follows:
In the mmwDemo_TransmitProcessedOutputTask function, I output all moving point clouds (speed greater than 0.5m/s) through the serial port:
I held the corner reflector away from and then closer to the radar at a speed of about 1.5m/s. There is no interference from other moving targets in the environment.
I found that the stable detection distance was only about 20 meters, but even at a position of 40 meters, the SNR was above 20.
Attached is the point cloud data. Are there other conditions that limit the detection results of point clouds?
point:20 frame:430
06 x 0.43 y:10.6 v 1.36 peak:72.0 snr:32.3
07 x 0.44 y:10.6 v 1.43 peak:69.7 snr:30.9
08 x 0.83 y:10.6 v 1.43 peak:69.7 snr:30.9
point:26 frame:431
06 x 0.55 y:10.6 v 1.39 peak:73.2 snr:33.0
07 x 0.50 y:10.6 v 1.45 peak:71.2 snr:33.4
08 x 0.50 y:10.6 v 1.45 peak:71.2 snr:33.4
09 x 0.22 y:10.9 v 1.35 peak:67.3 snr:28.1
10 x -0.12 y:10.9 v 1.47 peak:64.9 snr:26.3
point:27 frame:432
06 x 0.29 y:10.9 v 1.38 peak:70.7 snr:30.5
07 x 0.28 y:10.9 v 1.44 peak:68.8 snr:29.5
point:22 frame:433
07 x 0.65 y:11.0 v 1.52 peak:69.7 snr:28.1
08 x 0.56 y:11.0 v 1.61 peak:71.0 snr:31.5
point:29 frame:434
07 x 0.47 y:11.1 v 1.48 peak:69.8 snr:29.2
08 x 0.44 y:11.0 v 1.54 peak:70.0 snr:30.9
09 x 2.76 y:11.3 v 1.38 peak:68.6 snr:27.0
10 x 2.92 y:11.2 v 1.47 peak:67.2 snr:28.4
point:33 frame:435
07 x 0.25 y:11.2 v 1.49 peak:69.7 snr:30.9
08 x 0.10 y:11.2 v 1.55 peak:69.5 snr:32.0
09 x 0.53 y:11.2 v 1.55 peak:69.5 snr:32.0
10 x 1.49 y:11.9 v 1.28 peak:65.4 snr:26.4
11 x 1.52 y:11.9 v 1.52 peak:64.3 snr:26.2
point:29 frame:436
07 x 0.45 y:11.4 v 1.57 peak:67.4 snr:28.9
08 x 0.42 y:11.4 v 1.59 peak:68.5 snr:30.9
point:26 frame:437
08 x 0.18 y:11.5 v 1.45 peak:68.6 snr:28.4
09 x 0.58 y:11.5 v 1.45 peak:68.6 snr:28.4
10 x 0.51 y:11.5 v 1.65 peak:70.6 snr:31.2
point:24 frame:438
08 x 0.71 y:11.7 v 1.39 peak:69.7 snr:29.4
09 x 0.67 y:11.7 v 1.57 peak:70.3 snr:31.0
point:28 frame:439
09 x 0.29 y:11.9 v 1.23 peak:70.5 snr:31.4
10 x 0.35 y:11.8 v 1.39 peak:67.1 snr:28.6
point:21 frame:440
06 x 0.32 y:12.0 v 1.40 peak:70.0 snr:30.1
07 x 0.18 y:12.0 v 1.43 peak:67.9 snr:27.7
point:32 frame:441
07 x 0.43 y:12.2 v 1.51 peak:69.1 snr:29.5
08 x 0.43 y:12.2 v 1.54 peak:69.2 snr:30.5
point:23 frame:442
06 x 0.39 y:12.3 v 1.48 peak:71.2 snr:31.4
07 x 0.66 y:12.3 v 1.52 peak:70.8 snr:32.6
point:28 frame:443
10 x 0.57 y:12.5 v 1.45 peak:68.5 snr:29.6
11 x 0.38 y:12.5 v 1.51 peak:67.8 snr:28.9
point:34 frame:444
08 x 0.41 y:12.6 v 1.42 peak:69.2 snr:31.3
09 x 0.18 y:12.6 v 1.50 peak:68.2 snr:30.1
10 x 0.64 y:12.6 v 1.50 peak:68.2 snr:30.1
point:29 frame:445
07 x 0.46 y:12.7 v 1.47 peak:68.0 snr:28.7
08 x 0.56 y:12.8 v 1.54 peak:68.0 snr:28.4
point:34 frame:446
08 x 0.46 y:12.9 v 1.29 peak:66.1 snr:27.0
09 x 0.54 y:12.8 v 1.56 peak:66.8 snr:26.1
point:29 frame:447
09 x 0.50 y:13.1 v 1.41 peak:70.2 snr:29.9
10 x 0.51 y:13.0 v 1.44 peak:68.0 snr:27.4
point:26 frame:448
07 x 0.19 y:13.2 v 0.58 peak:68.7 snr:12.4
08 x 0.44 y:13.2 v 1.12 peak:69.4 snr:32.1
09 x 0.59 y:13.2 v 1.41 peak:65.3 snr:26.2
point:29 frame:449
07 x 0.52 y:13.2 v 0.55 peak:68.4 snr:11.9
08 x 0.62 y:13.3 v 1.13 peak:68.9 snr:29.3
09 x 0.62 y:13.3 v 1.13 peak:68.9 snr:29.3
10 x 0.64 y:13.3 v 1.40 peak:65.6 snr:26.7
point:32 frame:450
08 x 0.78 y:13.5 v 1.39 peak:66.5 snr:27.7
09 x 0.93 y:13.5 v 1.49 peak:65.4 snr:25.8
point:25 frame:451
07 x 0.83 y:13.6 v 1.42 peak:68.6 snr:27.1
08 x 0.72 y:13.6 v 1.50 peak:67.9 snr:27.1
point:31 frame:452
07 x 0.46 y:13.8 v 1.43 peak:69.5 snr:30.2
08 x 0.35 y:13.8 v 1.47 peak:68.2 snr:28.1
point:32 frame:453
08 x 0.59 y:13.9 v 1.40 peak:65.1 snr:26.7
09 x 0.84 y:13.9 v 1.46 peak:64.1 snr:25.0
point:26 frame:454
08 x 0.09 y:14.1 v 1.41 peak:68.0 snr:28.4
09 x 0.07 y:14.1 v 1.54 peak:68.0 snr:28.4
point:24 frame:455
06 x 1.44 y:14.3 v 1.41 peak:70.5 snr:30.9
07 x 1.30 y:14.3 v 1.54 peak:70.2 snr:32.3
point:28 frame:456
07 x 0.86 y:14.4 v 1.35 peak:72.6 snr:35.1
08 x 0.77 y:14.4 v 1.44 peak:70.4 snr:33.0
09 x -0.43 y:14.5 v 0.68 peak:67.2 snr:10.5
point:32 frame:457
08 x 0.91 y:14.6 v 1.28 peak:69.9 snr:31.2
09 x 0.75 y:14.6 v 1.45 peak:67.1 snr:28.2
point:25 frame:458
06 x 0.45 y:14.5 v 1.13 peak:66.5 snr:27.0
point:26 frame:459
07 x 0.26 y:14.7 v 1.20 peak:69.3 snr:29.4
08 x 0.32 y:14.7 v 1.37 peak:65.8 snr:26.3
point:26 frame:460
07 x 2.05 y:14.8 v 1.28 peak:65.1 snr:26.6
point:29 frame:461
07 x 0.33 y:15.0 v 1.27 peak:67.9 snr:28.6
08 x 0.38 y:15.0 v 1.46 peak:66.4 snr:27.4
point:27 frame:462
07 x 0.46 y:15.2 v 0.85 peak:66.5 snr:28.4
08 x 0.40 y:15.2 v 1.45 peak:64.6 snr:25.0
point:29 frame:463
06 x 0.80 y:15.3 v 0.93 peak:67.0 snr:28.9
07 x 0.63 y:15.3 v 1.47 peak:65.9 snr:27.7
point:27 frame:464
07 x 0.38 y:15.4 v 0.82 peak:65.4 snr:25.6
08 x 0.43 y:15.4 v 1.51 peak:64.2 snr:23.7
point:30 frame:465
08 x 0.59 y:15.6 v 0.90 peak:68.5 snr:31.1
09 x 0.54 y:15.6 v 1.53 peak:68.0 snr:29.6
point:32 frame:466
10 x -0.02 y:15.8 v 0.90 peak:69.7 snr:30.9
11 x 0.03 y:15.8 v 1.44 peak:67.4 snr:28.8
point:32 frame:467
11 x 0.01 y:16.0 v 1.02 peak:69.7 snr:30.5
12 x 0.30 y:16.0 v 1.37 peak:66.0 snr:26.9
point:27 frame:468
11 x 0.95 y:16.1 v 1.09 peak:66.1 snr:25.1
12 x 0.61 y:16.1 v 1.45 peak:64.5 snr:25.0
point:28 frame:469
11 x 1.02 y:16.3 v 1.32 peak:69.4 snr:30.5
12 x 1.08 y:16.3 v 1.49 peak:68.2 snr:26.8
point:28 frame:470
11 x 1.44 y:16.2 v 1.29 peak:69.3 snr:30.2
12 x 1.28 y:16.3 v 1.46 peak:67.9 snr:29.2
13 x 1.28 y:16.3 v 1.46 peak:67.9 snr:29.2
point:30 frame:471
11 x 2.38 y:16.5 v 1.42 peak:67.4 snr:28.5
point:25 frame:472
10 x 0.40 y:16.6 v 1.37 peak:67.5 snr:29.4
point:28 frame:473
11 x 1.10 y:16.5 v 1.31 peak:64.2 snr:24.0
12 x 1.35 y:16.6 v 1.49 peak:63.1 snr:24.0
point:26 frame:474
10 x 0.06 y:16.9 v 1.47 peak:66.8 snr:25.6
point:27 frame:475
11 x 0.14 y:17.1 v 1.36 peak:69.9 snr:29.5
12 x 0.00 y:17.1 v 1.46 peak:67.6 snr:28.2
point:23 frame:476
09 x 0.61 y:17.1 v 1.27 peak:64.6 snr:24.3
point:28 frame:477
11 x 0.01 y:17.3 v 1.32 peak:69.7 snr:27.1
12 x 0.05 y:17.3 v 1.39 peak:66.5 snr:26.1
point:30 frame:478
10 x 0.16 y:17.5 v 1.46 peak:68.3 snr:26.9
11 x 0.24 y:17.4 v 1.54 peak:68.4 snr:29.2
point:28 frame:479
10 x 0.30 y:17.6 v 1.34 peak:66.1 snr:23.6
11 x 0.49 y:17.6 v 1.51 peak:65.5 snr:24.5
point:29 frame:480
11 x 0.45 y:17.7 v 1.42 peak:69.6 snr:29.2
12 x 0.34 y:17.7 v 1.44 peak:67.6 snr:29.5
point:27 frame:481
11 x 1.86 y:17.8 v 1.32 peak:66.8 snr:27.2
12 x 1.61 y:17.9 v 1.50 peak:65.9 snr:24.5
point:25 frame:482
11 x 2.63 y:18.2 v 1.35 peak:65.4 snr:24.4
12 x 2.52 y:18.2 v 1.51 peak:64.5 snr:24.8
point:27 frame:483
10 x -1.33 y:18.2 v 1.41 peak:70.2 snr:29.0
11 x -1.62 y:18.1 v 1.49 peak:69.3 snr:30.3
point:25 frame:484
10 x 1.34 y:18.1 v 1.39 peak:66.4 snr:25.5
11 x 1.65 y:18.2 v 1.41 peak:64.3 snr:24.2
point:24 frame:485
10 x 0.73 y:18.5 v 1.29 peak:72.3 snr:31.6
11 x 0.69 y:18.5 v 1.35 peak:67.8 snr:27.7
point:27 frame:486
10 x 1.92 y:18.8 v 1.39 peak:71.1 snr:29.9
11 x 1.89 y:18.8 v 1.36 peak:67.2 snr:28.9
point:27 frame:487
10 x 0.81 y:18.7 v 1.26 peak:67.7 snr:26.8
11 x 0.85 y:18.7 v 1.47 peak:66.3 snr:26.7
point:27 frame:488
11 x 0.27 y:18.9 v 1.33 peak:73.2 snr:32.4
12 x 0.22 y:19.0 v 1.42 peak:70.7 snr:31.6
point:26 frame:489
10 x 0.06 y:19.0 v 1.30 peak:67.9 snr:25.9
11 x -0.10 y:19.0 v 1.46 peak:65.4 snr:24.8
point:30 frame:490
point:30 frame:491
10 x 1.27 y:19.3 v 1.39 peak:68.2 snr:28.3
11 x 1.19 y:19.3 v 1.48 peak:66.9 snr:29.2
point:29 frame:492
point:30 frame:493
10 x -1.61 y:19.5 v 1.25 peak:66.7 snr:26.7
11 x -1.53 y:19.5 v 1.43 peak:64.4 snr:23.8
12 x -1.53 y:19.5 v 1.43 peak:64.4 snr:23.8
point:24 frame:494
10 x 0.46 y:19.7 v 1.18 peak:70.7 snr:32.0
point:24 frame:495
10 x 2.03 y:19.8 v 1.15 peak:67.2 snr:26.4
point:25 frame:496
10 x 1.70 y:19.9 v 1.58 peak:61.9 snr:22.3
point:27 frame:497
10 x 0.39 y:20.1 v 1.19 peak:62.9 snr:23.4
point:22 frame:498
10 x -0.02 y:20.3 v 1.21 peak:66.7 snr:25.7
point:23 frame:499
point:23 frame:500
point:25 frame:501
10 x 1.98 y:20.5 v 1.35 peak:64.4 snr:26.6
11 x 1.72 y:20.5 v 1.48 peak:63.3 snr:24.0
point:23 frame:502
point:22 frame:503
point:27 frame:504
10 x 0.24 y:21.1 v 1.17 peak:64.8 snr:24.7
point:25 frame:505
11 x -1.17 y:21.2 v 0.88 peak:62.7 snr:22.5
12 x -0.18 y:21.2 v 0.88 peak:62.7 snr:22.5
point:25 frame:506
10 x 0.96 y:21.2 v 1.26 peak:62.8 snr:23.4
point:27 frame:507
point:27 frame:508
11 x 0.65 y:21.6 v 1.01 peak:64.4 snr:24.9
12 x 0.56 y:21.6 v 1.52 peak:63.6 snr:23.7
point:30 frame:509
point:28 frame:510
12 x 1.10 y:21.9 v 1.15 peak:64.1 snr:22.3
13 x 1.16 y:21.9 v 1.59 peak:65.3 snr:23.6
point:31 frame:511
12 x 0.98 y:22.1 v 1.10 peak:65.3 snr:25.1
13 x 1.78 y:22.0 v 1.10 peak:65.3 snr:25.1
14 x 1.00 y:22.0 v 1.50 peak:63.9 snr:24.4
15 x 1.85 y:22.0 v 1.50 peak:63.9 snr:24.4
point:27 frame:512
12 x 1.12 y:22.2 v 1.22 peak:64.6 snr:27.1
point:29 frame:513
13 x 0.23 y:22.4 v 1.32 peak:66.1 snr:25.9
point:26 frame:514
point:25 frame:515
10 x 0.44 y:22.7 v 1.39 peak:65.8 snr:24.6
11 x 0.43 y:22.7 v 1.61 peak:67.0 snr:27.3
point:27 frame:516
point:28 frame:517
10 x 0.30 y:23.0 v 1.46 peak:64.1 snr:25.7
11 x 0.02 y:23.0 v 1.55 peak:64.1 snr:25.6
point:25 frame:518
point:23 frame:519
point:26 frame:520
point:25 frame:521
point:27 frame:522
point:27 frame:523
12 x 0.98 y:23.8 v 1.56 peak:61.8 snr:21.8
point:26 frame:524
point:23 frame:525
point:27 frame:526
point:24 frame:527
point:25 frame:528
10 x 0.82 y:24.7 v 1.29 peak:64.5 snr:23.0
11 x 0.77 y:24.7 v 1.53 peak:64.3 snr:25.3
point:23 frame:529
point:25 frame:530
point:23 frame:531
point:23 frame:532
point:24 frame:533
point:25 frame:534
13 x 3.48 y:25.4 v 1.36 peak:66.0 snr:25.9
14 x 4.44 y:25.2 v 1.36 peak:66.0 snr:25.9
point:24 frame:535
point:26 frame:536
point:25 frame:537
13 x 1.51 y:26.0 v 1.47 peak:65.9 snr:27.0
14 x 2.61 y:26.1 v 1.26 peak:67.3 snr:27.6
point:27 frame:538
point:30 frame:539
point:27 frame:540
point:26 frame:541
point:25 frame:542
14 x 1.86 y:26.6 v 1.51 peak:65.1 snr:25.9
point:23 frame:543
point:24 frame:544
point:24 frame:545
12 x 0.54 y:27.1 v 1.59 peak:62.7 snr:21.7
point:22 frame:546
point:21 frame:547
point:22 frame:548
point:23 frame:549
point:28 frame:550
15 x 1.83 y:27.9 v 1.42 peak:65.2 snr:24.8
16 x 1.21 y:27.9 v 1.43 peak:62.9 snr:23.2
17 x 2.31 y:27.8 v 1.43 peak:62.9 snr:23.2
point:28 frame:551
14 x 0.23 y:27.9 v 1.37 peak:62.9 snr:24.5
point:24 frame:552
point:23 frame:553
point:28 frame:554
point:24 frame:555
point:25 frame:556
point:25 frame:557
13 x 1.84 y:28.8 v 1.27 peak:61.7 snr:21.1
point:27 frame:558
15 x -1.49 y:28.7 v 1.34 peak:63.8 snr:23.1
point:28 frame:559
16 x -0.91 y:28.8 v 1.36 peak:64.7 snr:23.9
point:22 frame:560
point:23 frame:561
point:23 frame:562
point:22 frame:563
point:25 frame:564
point:28 frame:565
point:27 frame:566
point:28 frame:567
point:27 frame:568
point:25 frame:569
point:27 frame:570
point:26 frame:571
point:25 frame:572
point:28 frame:573
point:26 frame:574
point:24 frame:575
point:25 frame:576
point:24 frame:577
point:24 frame:578
point:29 frame:579
point:29 frame:580
point:25 frame:581
point:29 frame:582
point:25 frame:583
point:26 frame:584
point:26 frame:585
point:26 frame:586
point:24 frame:587
point:22 frame:588
point:24 frame:589
point:27 frame:590
point:27 frame:591
point:26 frame:592
point:23 frame:593
point:27 frame:594
point:24 frame:595
point:25 frame:596
point:23 frame:597
point:25 frame:598
point:26 frame:599
point:23 frame:600
point:23 frame:601
point:23 frame:602
point:28 frame:603
point:26 frame:604
point:23 frame:605
point:22 frame:606
point:24 frame:607
point:26 frame:608
point:28 frame:609
point:26 frame:610
point:24 frame:611
point:25 frame:612
point:27 frame:613
point:21 frame:614
point:27 frame:615
point:25 frame:616
point:24 frame:617
point:24 frame:618
17 x 0.09 y:37.3 v 1.15 peak:62.9 snr:22.0
point:27 frame:619
point:26 frame:620
point:27 frame:621
point:25 frame:622
point:26 frame:623
point:25 frame:624
point:25 frame:625
point:24 frame:626
point:25 frame:627
point:23 frame:628
point:24 frame:629
point:24 frame:630
point:25 frame:631
point:28 frame:632
point:25 frame:633
point:23 frame:634
point:29 frame:635
point:23 frame:636
point:22 frame:637
point:27 frame:638
18 x 0.63 y:40.2 v 1.49 peak:65.0 snr:23.4
19 x 0.63 y:40.1 v 1.49 peak:65.0 snr:23.4
20 x 0.42 y:40.2 v 1.48 peak:64.0 snr:24.8
point:26 frame:639
point:24 frame:640
point:23 frame:641
point:24 frame:642
point:22 frame:643
point:22 frame:644
point:26 frame:645
19 x -0.39 y:41.2 v 1.33 peak:65.0 snr:22.9
point:24 frame:646
point:24 frame:647
point:24 frame:648
point:25 frame:649
17 x -0.14 y:41.6 v 1.40 peak:63.9 snr:24.0
point:24 frame:650
point:26 frame:651
point:23 frame:652
point:23 frame:653
point:24 frame:654
point:27 frame:655
point:24 frame:656
point:27 frame:657
point:23 frame:658
point:27 frame:659
point:23 frame:660
point:27 frame:661
point:25 frame:662
point:28 frame:663
point:23 frame:664
point:23 frame:665
point:27 frame:666
point:25 frame:667
point:26 frame:668
point:22 frame:669
point:24 frame:670
point:27 frame:671
point:23 frame:672
point:25 frame:673
point:25 frame:674
point:23 frame:675
point:25 frame:676
point:22 frame:677
point:25 frame:678
point:24 frame:679
point:26 frame:680
point:22 frame:681
point:27 frame:682
point:26 frame:683
point:27 frame:684
point:22 frame:685
point:25 frame:686
point:24 frame:687
point:25 frame:688
point:29 frame:689
point:24 frame:690
point:24 frame:691
point:26 frame:692
point:25 frame:693
point:25 frame:694
point:26 frame:695
point:26 frame:696
point:23 frame:697
point:30 frame:698
point:23 frame:699
point:23 frame:700
point:25 frame:701
point:23 frame:702
point:24 frame:703
point:23 frame:704
point:21 frame:705
point:27 frame:706
point:23 frame:707
point:25 frame:708
point:25 frame:709
point:25 frame:710
point:30 frame:711
point:28 frame:712
point:28 frame:713
point:27 frame:714
point:25 frame:715
point:27 frame:716
point:26 frame:717
point:28 frame:718
point:29 frame:719
point:27 frame:720
point:27 frame:721
point:25 frame:722
point:29 frame:723
point:25 frame:724
point:26 frame:725
point:24 frame:726
point:25 frame:727
point:27 frame:728
point:27 frame:729
point:27 frame:730
point:28 frame:731
point:28 frame:732
point:32 frame:733
point:31 frame:734
point:27 frame:735
point:24 frame:736
point:26 frame:737
point:29 frame:738
point:26 frame:739
point:30 frame:740
point:27 frame:741
point:27 frame:742
point:25 frame:743
point:31 frame:744
point:26 frame:745
point:27 frame:746
point:25 frame:747
point:26 frame:748
point:26 frame:749
18 x 0.97 y:40.2 v -1.89 peak:64.5 snr:25.0
point:27 frame:750
point:28 frame:751
point:25 frame:752
point:29 frame:753
point:26 frame:754
point:27 frame:755
point:28 frame:756
point:22 frame:757
point:24 frame:758
point:25 frame:759
point:24 frame:760
point:23 frame:761
16 x 0.20 y:38.2 v -1.78 peak:63.0 snr:22.7
point:21 frame:762
point:20 frame:763
point:23 frame:764
16 x 0.08 y:37.6 v -1.70 peak:64.2 snr:24.2
point:20 frame:765
point:21 frame:766
point:23 frame:767
point:27 frame:768
point:31 frame:769
point:26 frame:770
point:26 frame:771
point:26 frame:772
point:26 frame:773
point:24 frame:774
point:21 frame:775
point:26 frame:776
point:30 frame:777
point:22 frame:778
point:28 frame:779
point:26 frame:780
point:27 frame:781
21 x 0.73 y:34.5 v -1.97 peak:60.2 snr:20.8
22 x -0.19 y:34.5 v -1.94 peak:63.8 snr:23.4
point:25 frame:782
point:25 frame:783
point:28 frame:784
point:26 frame:785
point:28 frame:786
point:27 frame:787
point:31 frame:788
point:25 frame:789
point:25 frame:790
point:26 frame:791
point:32 frame:792
point:25 frame:793
point:25 frame:794
point:26 frame:795
point:27 frame:796
point:24 frame:797
point:27 frame:798
point:23 frame:799
point:21 frame:800
point:19 frame:801
point:23 frame:802
point:21 frame:803
point:16 frame:804
point:18 frame:805
point:19 frame:806
point:17 frame:807
10 x -0.36 y:29.9 v -1.68 peak:63.9 snr:23.6
point:16 frame:808
point:20 frame:809
point:18 frame:810
10 x -1.42 y:29.0 v -1.82 peak:64.7 snr:23.3
11 x -0.34 y:29.1 v -1.82 peak:64.7 snr:23.3
point:18 frame:811
11 x 0.36 y:29.3 v -1.75 peak:62.8 snr:23.5
point:22 frame:812
13 x 1.22 y:28.9 v -1.67 peak:62.3 snr:23.6
point:22 frame:813
point:18 frame:814
09 x 0.27 y:28.7 v -1.57 peak:65.9 snr:24.4
10 x -0.02 y:28.9 v -1.56 peak:65.4 snr:24.0
point:18 frame:815
10 x 0.96 y:28.6 v -1.78 peak:64.0 snr:24.9
point:15 frame:816
point:19 frame:817
point:15 frame:818
point:18 frame:819
point:18 frame:820
point:15 frame:821
point:17 frame:822
point:17 frame:823
point:22 frame:824
14 x 2.98 y:27.0 v -1.65 peak:61.9 snr:22.3
15 x 2.98 y:27.0 v -1.65 peak:61.9 snr:22.3
point:20 frame:825
point:22 frame:826
point:23 frame:827
point:18 frame:828
point:25 frame:829
point:25 frame:830
point:21 frame:831
point:21 frame:832
point:22 frame:833
point:29 frame:834
14 x 0.69 y:25.3 v -1.73 peak:66.2 snr:27.6
15 x 0.75 y:25.3 v -1.44 peak:62.7 snr:24.2
point:22 frame:835
10 x 1.79 y:25.2 v -1.87 peak:65.0 snr:24.8
point:23 frame:836
10 x 1.52 y:25.0 v -1.82 peak:67.8 snr:28.3
point:21 frame:837
point:23 frame:838
10 x 0.22 y:24.6 v -1.73 peak:67.8 snr:28.6
point:21 frame:839
point:22 frame:840
09 x 0.82 y:24.1 v -1.87 peak:64.3 snr:25.7
point:24 frame:841
11 x 0.05 y:24.0 v -1.68 peak:66.3 snr:25.8
point:25 frame:842
10 x -0.94 y:23.9 v -1.53 peak:63.9 snr:23.6
11 x -1.01 y:23.9 v -1.53 peak:63.7 snr:23.2
point:22 frame:843
point:26 frame:844
10 x -0.03 y:23.5 v -1.83 peak:64.3 snr:23.5
point:25 frame:845
10 x -0.13 y:23.3 v -1.89 peak:67.3 snr:28.5
point:26 frame:846
10 x -0.53 y:23.2 v -1.79 peak:65.9 snr:26.1
11 x -0.78 y:23.3 v -1.62 peak:61.8 snr:22.1
point:21 frame:847
09 x 0.40 y:23.0 v -1.61 peak:65.7 snr:24.1
point:24 frame:848
10 x 0.36 y:22.9 v -1.67 peak:65.1 snr:25.8
point:21 frame:849
09 x 0.73 y:22.6 v -1.87 peak:65.4 snr:26.0
point:25 frame:850
12 x -0.85 y:22.5 v -1.79 peak:68.1 snr:26.9
point:32 frame:851
point:25 frame:852
point:29 frame:853
14 x 0.73 y:21.9 v -1.70 peak:63.1 snr:23.1
point:34 frame:854
15 x 0.48 y:21.8 v -1.96 peak:64.7 snr:24.0
16 x -0.36 y:21.8 v -1.88 peak:69.1 snr:27.9
17 x 0.52 y:21.9 v -1.88 peak:69.1 snr:27.9
18 x -0.40 y:21.9 v -1.26 peak:62.1 snr:21.8
point:33 frame:855
15 x 0.11 y:21.7 v -1.86 peak:65.6 snr:26.3
point:28 frame:856
10 x 0.48 y:21.4 v -1.68 peak:65.5 snr:28.3
point:24 frame:857
point:26 frame:858
09 x 0.09 y:21.2 v -1.91 peak:62.3 snr:23.4
10 x -0.12 y:21.2 v -1.78 peak:68.3 snr:29.2
point:26 frame:859
point:29 frame:860
10 x 0.46 y:20.7 v -1.68 peak:64.2 snr:25.4
point:28 frame:861
11 x 0.41 y:20.6 v -1.58 peak:65.2 snr:25.3
12 x 0.51 y:20.6 v -1.37 peak:63.8 snr:23.6
point:29 frame:862
point:29 frame:863
09 x 0.62 y:20.2 v -1.77 peak:64.7 snr:25.5
point:28 frame:864
10 x 0.22 y:20.1 v -1.86 peak:65.5 snr:27.2
point:28 frame:865
09 x -0.37 y:19.9 v -1.75 peak:65.7 snr:24.2
point:27 frame:866
10 x 0.47 y:19.5 v -1.65 peak:64.4 snr:24.2
point:28 frame:867
09 x 0.88 y:19.6 v -1.67 peak:66.5 snr:25.3
10 x 0.81 y:19.6 v -1.41 peak:63.9 snr:22.8
point:26 frame:868
10 x -0.05 y:19.4 v -1.77 peak:66.9 snr:27.5
point:27 frame:869
point:26 frame:870
12 x 0.44 y:19.0 v -1.66 peak:66.5 snr:26.6
point:24 frame:871
point:30 frame:872
10 x 0.27 y:18.7 v -1.58 peak:66.3 snr:27.2
11 x 0.20 y:18.7 v -1.43 peak:65.5 snr:25.3
point:27 frame:873
11 x 0.31 y:18.5 v -1.76 peak:67.6 snr:27.1
point:37 frame:874
13 x 0.08 y:18.4 v -1.83 peak:69.0 snr:29.6
14 x 0.04 y:18.4 v -1.65 peak:63.3 snr:22.0
point:31 frame:875
03 x 2.30 y: 6.3 v -0.73 peak:62.6 snr:22.4
12 x 0.03 y:18.2 v -1.74 peak:67.1 snr:26.6
point:30 frame:876
11 x -0.05 y:18.0 v -1.66 peak:68.7 snr:27.6
12 x 0.09 y:18.0 v -1.56 peak:66.1 snr:26.1
point:36 frame:877
12 x 0.45 y:17.9 v -1.71 peak:68.7 snr:28.7
13 x 0.31 y:17.9 v -1.60 peak:65.4 snr:22.4
point:34 frame:878
13 x 0.18 y:17.7 v -1.84 peak:67.0 snr:26.2
point:35 frame:879
15 x 1.41 y:17.5 v -1.73 peak:65.6 snr:24.2
point:30 frame:880
12 x 0.44 y:17.4 v -1.68 peak:68.6 snr:27.1
13 x 0.61 y:17.4 v -1.59 peak:66.1 snr:24.9
point:29 frame:881
06 x 0.54 y:17.2 v -1.59 peak:65.4 snr:26.2
07 x 0.75 y:17.2 v -1.46 peak:65.0 snr:23.3
point:31 frame:882
10 x 0.54 y:17.0 v -1.54 peak:65.2 snr:25.0
point:30 frame:883
10 x 1.03 y:16.9 v -1.73 peak:67.1 snr:27.3
11 x 1.19 y:16.9 v -1.56 peak:63.4 snr:22.6
point:30 frame:884
09 x -0.34 y:16.7 v -1.85 peak:66.4 snr:27.1
point:28 frame:885
09 x 0.63 y:16.4 v -1.79 peak:65.4 snr:25.2
point:29 frame:886
10 x 0.10 y:16.3 v -1.71 peak:69.9 snr:29.5
11 x 0.15 y:16.3 v -1.43 peak:66.7 snr:24.7
point:28 frame:887
03 x 1.01 y: 4.8 v -1.14 peak:64.4 snr:24.9
04 x 1.17 y: 4.8 v -1.14 peak:64.4 snr:24.9
point:30 frame:888
point:29 frame:889
08 x 0.62 y:15.7 v -1.73 peak:67.7 snr:27.9
09 x 0.22 y:15.7 v -0.88 peak:64.5 snr:24.2
10 x 0.83 y:15.7 v -0.88 peak:64.5 snr:24.2
point:28 frame:890
08 x 1.44 y:15.5 v -1.61 peak:67.5 snr:27.8
09 x 1.05 y:15.6 v -0.89 peak:66.0 snr:25.0
point:28 frame:891
07 x 0.38 y:15.4 v -1.57 peak:67.4 snr:27.4
08 x 0.39 y:15.4 v -0.94 peak:66.9 snr:26.0
point:29 frame:892
06 x 1.25 y:15.3 v -1.63 peak:68.2 snr:27.4
07 x 1.26 y:15.3 v -0.97 peak:66.6 snr:24.7
point:27 frame:893
06 x 0.18 y:15.1 v -1.75 peak:69.4 snr:30.4
07 x 0.20 y:15.1 v -1.41 peak:65.4 snr:24.9
point:31 frame:894
07 x 0.67 y:15.0 v -1.88 peak:64.5 snr:25.2
08 x 0.81 y:15.0 v -1.76 peak:71.4 snr:32.5
09 x 0.76 y:15.0 v -1.46 peak:67.1 snr:27.2
point:28 frame:895
07 x 0.16 y:14.7 v -1.79 peak:67.5 snr:27.5
point:28 frame:896
06 x 1.12 y:14.7 v -1.68 peak:71.1 snr:32.1
07 x 1.12 y:14.7 v -1.39 peak:68.2 snr:28.3
point:29 frame:897
03 x 1.42 y: 3.5 v -0.93 peak:67.1 snr:23.7
07 x 0.49 y:14.4 v -1.66 peak:69.4 snr:30.0
08 x 0.65 y:14.4 v -1.46 peak:66.9 snr:28.5
point:31 frame:898
06 x 0.69 y:14.2 v -1.92 peak:64.8 snr:27.4
07 x 0.61 y:14.2 v -1.84 peak:70.2 snr:30.9
08 x 0.59 y:14.1 v -1.52 peak:64.2 snr:23.1
point:28 frame:899
06 x 0.49 y:14.0 v -1.76 peak:68.8 snr:31.2
point:28 frame:900
06 x 0.33 y:14.0 v -1.88 peak:63.6 snr:24.9
07 x 0.39 y:14.0 v -1.68 peak:71.8 snr:32.8
08 x 0.66 y:14.0 v -1.55 peak:69.3 snr:29.8
09 x 0.66 y:14.0 v -1.55 peak:69.3 snr:29.8
point:28 frame:901
06 x 0.58 y:13.7 v -1.58 peak:70.3 snr:30.4
07 x 0.48 y:13.7 v -1.55 peak:69.5 snr:28.9
point:34 frame:902
06 x 0.08 y:13.6 v -1.69 peak:71.1 snr:32.2
07 x 0.11 y:13.6 v -1.62 peak:67.9 snr:29.0
point:27 frame:903
06 x 0.31 y:13.4 v -1.92 peak:65.3 snr:26.9
07 x 0.39 y:13.4 v -1.81 peak:71.0 snr:32.6
08 x 0.45 y:13.4 v -1.42 peak:65.6 snr:28.1
point:31 frame:904
06 x 0.46 y:13.2 v -1.79 peak:69.7 snr:31.7
07 x 0.79 y:13.2 v -1.36 peak:64.7 snr:25.6
point:30 frame:905
06 x 0.11 y:13.0 v -1.90 peak:64.0 snr:24.2
07 x 0.29 y:13.0 v -1.77 peak:71.0 snr:31.6
08 x 0.38 y:13.0 v -1.44 peak:65.9 snr:25.7
point:29 frame:906
06 x 0.50 y:12.9 v -1.68 peak:70.0 snr:29.9
07 x 0.62 y:12.9 v -1.38 peak:67.2 snr:26.3
point:33 frame:907
02 x 1.34 y: 2.3 v -0.58 peak:64.9 snr:22.3
07 x 0.49 y:12.7 v -1.89 peak:65.5 snr:25.5
08 x 0.48 y:12.7 v -1.77 peak:72.3 snr:32.7
09 x 0.38 y:12.7 v -1.69 peak:67.6 snr:27.0
point:35 frame:908
06 x 0.59 y:12.5 v -1.92 peak:64.9 snr:25.8
07 x 0.59 y:12.5 v -1.92 peak:64.9 snr:25.8
08 x 0.56 y:12.5 v -1.83 peak:70.4 snr:30.8
09 x 0.57 y:12.6 v -1.69 peak:64.5 snr:24.8
point:33 frame:909
00 x 1.42 y: 2.0 v -0.62 peak:67.6 snr:25.1
07 x 0.08 y:12.4 v -1.88 peak:63.9 snr:23.2
08 x 0.18 y:12.4 v -1.73 peak:71.3 snr:30.9
09 x 0.32 y:12.4 v -1.62 peak:67.7 snr:25.9
point:23 frame:910
06 x 0.40 y:12.2 v -1.65 peak:71.1 snr:31.9
07 x 0.61 y:12.2 v -1.53 peak:69.1 snr:28.6
point:24 frame:911
06 x 0.34 y:12.0 v -1.60 peak:72.7 snr:32.9
07 x 0.33 y:12.0 v -1.58 peak:71.4 snr:30.7
point:29 frame:912
07 x 0.51 y:11.9 v -1.88 peak:62.7 snr:25.2
08 x 0.54 y:11.9 v -1.69 peak:71.3 snr:32.2
09 x 0.62 y:11.9 v -1.53 peak:68.1 snr:26.8
point:29 frame:913
06 x 0.31 y:11.6 v -1.92 peak:66.9 snr:28.4
07 x 0.24 y:11.6 v -1.86 peak:71.9 snr:30.6
08 x 0.16 y:11.7 v -1.51 peak:65.5 snr:24.7
09 x 2.67 y:12.0 v -1.79 peak:68.2 snr:26.7
point:35 frame:914
06 x 0.54 y:11.4 v -1.84 peak:71.2 snr:31.7
07 x 0.54 y:11.5 v -1.84 peak:71.2 snr:31.7
08 x 0.48 y:11.4 v -1.64 peak:65.3 snr:26.2
09 x 2.93 y:11.6 v -1.54 peak:65.6 snr:26.4
point:27 frame:915
07 x 0.28 y:11.3 v -1.89 peak:65.6 snr:26.8
08 x 0.14 y:11.3 v -1.75 peak:73.0 snr:34.2
09 x 0.17 y:11.3 v -1.63 peak:68.6 snr:28.4
point:28 frame:916
06 x 0.16 y:11.2 v -1.86 peak:66.2 snr:26.2
07 x 0.59 y:11.2 v -1.86 peak:66.2 snr:26.2
08 x 0.53 y:11.2 v -1.71 peak:73.9 snr:33.4
09 x 0.49 y:11.2 v -1.55 peak:70.7 snr:31.0
point:28 frame:917
07 x 0.30 y:10.9 v -1.90 peak:66.4 snr:27.2
08 x 0.30 y:10.9 v -1.79 peak:72.6 snr:33.0
09 x 0.29 y:10.9 v -1.70 peak:67.5 snr:26.3
point:30 frame:918
06 x 0.42 y:10.8 v -1.78 peak:72.3 snr:32.9
07 x 0.45 y:10.8 v -1.65 peak:67.5 snr:25.5
point:23 frame:919
06 x 0.07 y:10.7 v -1.86 peak:66.1 snr:27.6
07 x 0.21 y:10.6 v -1.72 peak:73.8 snr:33.9
08 x 0.53 y:10.6 v -1.65 peak:70.3 snr:30.3
point:23 frame:920
06 x 0.29 y:10.4 v -1.60 peak:71.3 snr:32.1
07 x 0.13 y:10.4 v -1.56 peak:69.6 snr:28.8
08 x 0.55 y:10.4 v -1.56 peak:69.6 snr:28.8
Thanks!