Hi,
I see that in the Cascade_Phase_Shifter_Calibration_AWRx.lua script, the sensors are configured in a loop from phase shifter value 0 to 63 which are in steps of 5.625 degrees. This translates to phases going from 0 to 354.275 (i.e. 360 - 5.625) degrees. In the TXBF_PS_LUT_Generate.m script, the theta value is -15:deltaTheta:15 where deltaTheta = 1.0. How can the full phase shifter range translate to a 30 degree beam?