Other Parts Discussed in Thread: AWR6843AOP
Hello TI Forum,
I had followed the CSS Debug process for debugging AWR6843AOP which is mentioned at Using CCS Debug
Below are the setup images that I am using. S3 of EVM is set to Off.
I had tested the JTAG connecting using the test present at target while creating a target configuration I can see the tests are successfully.
When I try running debug the following below error is showed in the console and unable to move forward to breakpoint that I had set.
Cortex R4 0: Trouble Setting Breakpoint with the Action "Process CIO at exte962: (Error 18650x1E964) Unable to access device memory. Verify that the memory address is in valid memory. Herron persists, confirm configuration, power cycle board, and/or try more reliable JTAG settings (eg. lower TCLK). (Emulation package 9.12.0.00150) Cortex R4 0: Breakpoint Manager: Retrying with a AET breakpoint
Cortex R4 : Trouble Setting Breakpoint with the Action "Terminate Program Execution at 0x20518 (Error -1065@ 8x20514) Unable to access device memory. Verify that the memory address is in valid memory. It error persists, confire configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLE). (Emilation package 9.12.0.00156) Cortex R4 0: Breakpoint Manager: Retrying with a AET breakpoint
I had turned off the optimisations aswell.
Moreever I am unable to use CLI for sending the config in order to start the sensor.
Thank You.