This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: mmWave Demo Visualizer

Part Number: IWR1443BOOST


We are currently checking the detection of IWR1443BOOST using mmWave Demo Visualizer.

1. Please show us the data structure of the file output by clicking the RECORD START button on the plots screen in mmWave Demo Visualizer.

2.When detecting the liquid level in a tank using IWR1443BOOST, it is said that the detection data can be obtained from UART,

  but please provide a sample program (language used: C, C++, Python) and a configuration file.

Thank you.

  • Hi,

    1.Can you please send a snapshot of where you see "RECORD START" in mmwave demo visualizer?

    2.You can find the sample cfg file at radar_toolbox_1_20_00_11\source\ti\examples\Level_Sensing\high_accuracy\chirp_configs\high_accuracy_demo_14xx

    You can find the source code of the application at radar_toolbox_1_20_00_11\source\ti\examples\Level_Sensing\high_accuracy\src\14xx

    MmwDemo_transmitProcessedOutput() in main.c will provide details about the TLV format

    Regards,

    Abhishek