This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error when loading a cfg file in the Industrial Visualizer when using gui_main.py

Part Number: IWR6843ISK


Hey there,

I´m using the Industrial Visualizer with the "Vital Signs with People Tracking" demo. When I launch the Industrial_Visualizer.exe everything works fine.

For my project I want to modify the visualizer code. Now everytime I try to load the cfg file (vital_signs_ISK_2m) into the gui, which I started from the gui_main.py file, I get the following errors and the config is not loaded.

This is with the unedited code and happened on two different machines. I hope you can help me fix this.

Thanks