This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Are ferrite beads needed with the LP87745 PMIC/Switcher

Part Number: IWR6843
Other Parts Discussed in Thread: LP87745, LP87745-Q1

Do I need to add the ferrite beads to the switcher outputs from the LP87745? I am looking for the maximum range on the IWR6843, but I thought the 17.6 Mhz switching would eliminate the need for additional ferrite bead filtering.

Thanks-

Mike Schell