What is the maximum current that can be drawn from the DVDD regulator to power an external device?
I have a microcontroller that runs of 1.8V and uses 0.7mA. Using the internal DVDD regulator of the PGA305 would save me quite a bit of PCB space.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the maximum current that can be drawn from the DVDD regulator to power an external device?
I have a microcontroller that runs of 1.8V and uses 0.7mA. Using the internal DVDD regulator of the PGA305 would save me quite a bit of PCB space.
Hi Gaurav Hirlekar,
I understand the desire to want to use the DVDD as a power source, but it is not recommended. The DVDD regulator is designed for the the PGA305 itself and not designed to power other devices. The reason for the output pin is to be able to connect a required bypass capacitor on the DVDD supply. The DVDD output pin is not meant to supply other devices.
Best regards,
Bob B