This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST-ODS: AWR1642BOOST-ODS

Part Number: AWR1642BOOST-ODS

Hi I'm Bhavya

we are using Code composer studio version 9 and tried to compile the sample example project which is  for 1642

and I'm getting the following errors.in

obstacle detection 

 odsdemo_16xx_mss

  • "../mss_main.c", line 1594: error #167: too few arguments in function call
    1 error detected in the compilation of "../mss_main.c".
    gmake[1]: *** [mss_main.obj] Error 1
  • gmake[1]: Target 'main-build' not remade because of errors.
    Finished building: "../cli.c"

    makefile:152: recipe for target 'all' failed
    gmake: *** [all] Error 2

odsdemo_16xx_dss

  • subdir_rules.mk:9: recipe for target 'odsdemo_aoaEstBF2D.oe674' failed
    "C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/utils/mmwDemo_monitor.h", line 64: error #102: "MmwDemo_AnaMonitorCfg_t" has already been declared in the current scope
    "C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/utils/mmwDemo_monitor.h", line 71: error #258: invalid redeclaration of type name "MmwDemo_AnaMonitorCfg" (declared at line 366 of "..\./common/mmw_config.h")
    2 errors detected in the compilation of "../odsdemo_aoaEstBF2D.c".
    gmake[1]: *** [odsdemo_aoaEstBF2D.oe674] Error 1
  • "C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/utils/mmwDemo_monitor.h", line 64: error #102: "MmwDemo_AnaMonitorCfg_t" has already been declared in the current scope
    "C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/utils/mmwDemo_monitor.h", line 71: error #258: invalid redeclaration of type name "MmwDemo_AnaMonitorCfg" (declared at line 366 of "C:/Workspace/code composer/odsdemo_16xx_dss/./common/mmw_config.h")
    "../dss_main.c", line 118: error #20: identifier "MMWAVE_L3RAM_NUM_BANK" is undefined
    "../dss_main.c", line 118: error #20: identifier "MMWAVE_SHMEM_BANK_SIZE" is undefined
    4 errors detected in the compilation of "../dss_main.c".
    gmake[1]: *** [dss_main.oe674] Error 1
  • "C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/utils/mmwDemo_monitor.h", line 64: error #102: "MmwDemo_AnaMonitorCfg_t" has already been declared in the current scope
    "C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/utils/mmwDemo_monitor.h", line 71: error #258: invalid redeclaration of type name "MmwDemo_AnaMonitorCfg" (declared at line 366 of "..\./common/mmw_config.h")
    2 errors detected in the compilation of "../odsdemo_clusteringDBscan3D.c".
    gmake[1]: *** [odsdemo_clusteringDBscan3D.oe674] Error 1
  • gmake[1]: Target 'main-build' not remade because of errors.
    Finished building: "../odsdemo_heatmap.c"

    makefile:161: recipe for target 'all' failed
    gmake: *** [all] Error 2

level sensing-high accuracy

high_accuracy_16xx_mss-----can't open mmw_config.h.

nonos_oob_16xx----"C:/Workspace/code composer/AWR16xx_dss_nonOS/dss_data_path.h", line 44: fatal error #1965: cannot open source file "ti/demo/io_interface/mmw_config.h