Other Parts Discussed in Thread: TI-SCB
I am asking you because there is a problem in the process of sensor testing using the TMAG5170UEVM_GUI program by purchasing two TMAG5170UEVM boards and TI-SCB boards.
One TMAG5170UEVM is recognized as a TMAG5170A2 board when both TMAG5170A1 and TMAG5170A2 are connected, and I entered the register to change it to Active measure mode, but all registers are displayed as 0xFFFF and register value cannot be changed.
The other TMAG5170UEVM was recognized as a TMAG5170APLEVM board when the TMAG5170A1 and TMAG5170A2 were connected respectively, which did not have an Active measurement mode and could not measure the magnetic field strength.
All firmware updates have been completed, and retrying after pressing the reset button on the TI-SCB did not resolve.
I would appreciate it if you could tell me the cause and solution to this problem.