This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: SDK supported command/parameter

Part Number: AWR2944


Hello,

     Is CLI command/parameter guideline of SDK mmwave_mcuplus_sdk_04_04_01_02 available?

EX:

"chirpCfg 0 0 0 0 0 0 0 1 \n\r",
"chirpCfg 1 1 0 0 0 0 0 4 \n\r",
"frameCfg 0 1 16 0 656 100 1 0 \n\r",
"lowPower 0 0 \n\r",
"guiMonitor -1 1 1 0 0 0 1 \n\r",
"cfarCfg -1 0 2 8 4 3 0 15 1 \n\r",
"cfarCfg -1 1 0 4 2 3 1 15 1 \n\r",
"multiObjBeamForming -1 0 0.5 \n\r",
"calibDcRangeSig -1 0 -5 8 256 \n\r",
"clutterRemoval -1 0 \n\r",
"compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 \n\r",

Thank you!

Edward

  • Hello Edward,

    You can go to: C:\ti\mmwave_mcuplus_sdk_04_04_01_02\mmwave_mcuplus_sdk_04_04_01_02\docs\mmwave_mcuplus_sdk_user_guide.pdf
    There in the section 3.6: Configuration (.cfg) File Format (For DDMA commands, refer to the DDMA Documentation)
    You can find all the details.

    Regards,
    Saswat Kumar