We are working with the AWR2243 Cascade board Lua scripts that are provided with the mmwave studio generation 2. To perform a SIMO, we have been editing the following scripts: Cascade_Configuration_TestSource.lua (mostly this one) and Cascade_Capture.lua. We would like to know where the methods in these codes are defined such as ChirpConfig_mult. We would also like to know what exactly constitutes a SIMO configuration as opposed to a MIMO. Does a SIMO configuration mean that only the master device has a singular TX enabled and all 4 RX enabled while all the slaves have all of the TXs disabled with the 4 RX enabled? Or is there one TX enabled for each device with all of the RX enabled?