Hi there,
From the AWR2243 datasheet, when using the LVDS output interface, the LVDS clock can run up to 450 MHz = 900 Mbps per lane (section 8.9.6). When using the CSI-2 interface, the CSI-2 clock can run up to 300 MHz = 600 Mbps per lane (section 8.9.8.1). Could you comment on the difference in max LVDS clock speed vs. max CSI-2 clock speed? Is there a way to run the CSI-2 interface faster than 300 MHz?
Thanks,
Kyle