This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Frequency calibration of MMW cascaded radar

Part Number: AWR2243
Other Parts Discussed in Thread: TIDEP-01012

TI user guides suggest performing frequency calibration of the multi-chip radar systems due to imperfectly consistent transmit frequency and the frequency chirp slope. The correction is to be applied to the time domain/ADC data prior to phase calibration and beam forming. The correction equation requires experimental evaluation of the frequency and chirp rate variations, possibly separate for different MMW operation frequencies.

It is not clear what can be the origin of the TX frequency difference and the chirp rate since all cascaded chips are driven by 20GHz master chirps and x4 multipliers. Is it because the MMW frequencies are not simple harmonics and there are some frequency control loops involved in each chip? That would explain some frequency difference but not the mean slope, although it can slightly vary over duration of the chirp. Please clarify, since e.g TI Signal Processing User Guide_4chipCascade doc Fig.14 shows experimental data suggesting that variations are real.

Please describe some details regarding frequency variation measurements among VR channels. Does it require transmission of single tones and external MMW spectrum analyzer? The above mentioned user guide shows FFT in the range domain, but that would require transmitting chirping signals and is related to the chirp rate rather than frequency as suggested by the Fig.14 description. In addition, some variations in the peak location could be attributed to the range difference between target and the VR channel location if the target is too close. Please clarify. A tutorial would be helpful.

For the same reason as above it is not clear how the chirp rate can be different among different chips. An explanation and a guide how to estimate the rate variations would be helpful.

It also appears that TI team recommends to generate multiple calibration matrices for different beam angles in order to improve beam quality. Is it the case?

Thank you in advance.

  • Hi,

    Please let us know what TI documents in addition to "TI Signal Processing User Guide_4chipCascade doc" you are referring to

    thank you

    Cesar

  •  Hi Cesar,

    A brief description of frequency calibration is in:
    Design Guide: TIDEP-01012
    Imaging Radar Using Cascaded mmWave Sensor
    Reference Design

    But the 2020 reference that I mentioned in my questions provides more detail description. I does not appears in TI repository anymore, but I've read about it on e2e forum and have found that doc here:

    https://vdocuments.mx/signal-processing-with-4-chip-cascade.html?page=1

    The current and the old guides suggest that frequency calibration is required to improve performance of the cascaded radar. We have ignored this step and not sure why it is needed since all chips are driven by common chirp pulses at 20GHz. Our calibration only includes phase by collecting signals reflected from a cube retroreflector after range FFTs in virtual channels.

    We are trying to understand reasons for this requirement and how TI collects data for its implementation.

    Thank you.

  • Hi,

    Sorry for the delay

    The document you mentioned is provided in the mmwave studio release:

    C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples\signal_processing_4chip_cascade.pdf

    I think you are referring section "5.1.1 Frequency mismatch"

    The cause of the frequency mismatch is the mismatch in the line length between the different Rx antennae.

    The frequency mismatch is not as important as the phase mismatch.

    If you are meeting your performance requirements we don't recommend to perform it

    thank you

    Cesar

  • Cesar,

    Thanks for the comment.