Hi TI Support team,
I am getting error message “ Flash unsuccessful” when trying to update the firmware. My setup is consisting of INA228EVM connected to SCB board and USB cable that was supplied in the package connected to the laptop. I have installed the GUI interfaces and I can successfully connect to the TI_SCB.
I have followed all the steps per user guide but unable to update the firmware.
Can you please provide the proper steps on how to update the firmware?
Also, the IN228EVM that I have received has SW0 and SW1 with a 4-position switch for each. The silk screen on the PCB for these switches do not match what is shown in the user guide document.
On my board the 4 positions are shown as GND, VS, SDA & SCL. In the user guide the INA228EVM has only one 4 position switch and positions are labeled as CS1, CS2, CS3 & CS4.
This is very confusing. The GUI interface configuration page has SW1 and SW2 HW configuration settings and the option to select are CS1, CS2, CS3 & CS4.
It’s not clear how I select the switch setting on the INA228EVM board to match the switch configuration on the GUI interface.
Please proved explanation on how to configure the switch setting on the board “GND, VS, SDA & SCL” to correspond to “CS1, CS2, CS3 & CS4”?