We are now check the temperature of AWRL6432 module using the internal temp sensor and thermo-camera.
In the result of three module, the difference between the internal sensor value and IC top temperature would be about 10degrees.
The thermal resistance between junction and package top is 0.36, so then we are considering that the difference is too big.
So then, we have some question,
・How much is the error of temperature sensor in AWRL6432?
・The internal sensor value would be higher than actual tenperature?
・The meaning of "error" is the difference every IC?
・How about repeatability in case of using same IC?
The power consumption: 300mW at 25degrees
Best regards,
Tak