Other Parts Discussed in Thread: IWR1443
Dear sir
I have heard that when I send a Configuration File from the PC to the IWR1443BOOST through serial communication (USB, UART) between the IWR1443BOOST and the PC, the detection data is returned from the IWR1443BOOST.
Is it okay to use one COM port in this case? If two are required, how should they be used?For example, will COM5 be the configuration sending port from the PC to IWR1443BOOST, and COM4 be the detection data receiving port from IWR1443BOOST?
Please kindly advise.
P.S.
I have been inquiring about a resource site regarding Configuration File for some time, but I cannot find it using the information you have provided (site address).
It's been more than 3 weeks since I contacted you. If possible, please show me how to write a configuration file or a sample file.
Thank you.
Hiromichi