This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: Acquired data download from SSD

Part Number: TIDEP-01012


Hello,

I made some acquisition with TIDEP 01012 in MIMO configuration such that I could acquire as much frame as possible taken at 2.5 ms. I saw that final .bin files on SSD are quite large and since the WinSCP tool seems to be very slow (I found also on the forum other people complaining it), I was asking if there's any other method to download acquired data, like USB or any other method via Ethernet.

Thank you,

Federico