Hi,
After triggering warm reset, the device starts from the RBL. See AWR2944: Where will device start from after triggering warm reset - Sensors forum - Sensors - TI E2E support forums
/* Warm reset */
/*
* topRCM->SOFTSYSRST Register (Offset = 1Ch) [reset = 0h]
* Write 0xAD to trigger warm reset to the chip..
*/
uint32_t* regAddr = (uint32_t*)0xFFFFE11C;
*regAddr = 0xAD;
However, in this case, the RBL does not reload the MetaImage 1 from the external flash. So, Can I reset the IWR6843AoP in software and force the RBL to load Meta Image 1 from external Flash again?
Background: We would like to restart the SBL with a software command from the application code to start the update process.
Best Regards,
Robin