Other Parts Discussed in Thread: OPT3001
Hello, I bought the OPT4001EVM for a project and am trying to connect it with a microcontroller and have that provide power as well.
However, it seems that approach does not work with the motherboard that comes with the part. With that in mind, I detached the coupon board in order to use that and set it up with an Arduino Nano. The problem now is that I am just getting 0 for my Lux values. Any ideas? I have VDD, SDA, SCL and GND connected, with the ADDR pin set to GND. Additionally, I made sure I had pull up resistors for the I2C bus (10k ohms).