This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC3021:How to do Bake/Rehydration, for which conditions it is necessary

Part Number: HDC3021

I would like to ask my questions item by item.
1- Do both Baking/Rehydration need to be done together? is it enough if I do Rehydration?
2-Is it necessary to do Baking/Rehydration after smd assembly? What happens if I don't or if I do, will it help for sensitivity ?
3- did the sensitivity values given after smd assembly or after Baking/Rehydration in datasheet?
4- In which cases Baking/Rehydration process should be done.

  • Hello,

    1. Baking removes moisure from the polymer on top of the sensor, and rehydration restores moisture. So they are not performed together, but at different times as needed

    2. After soldering/assembly, rehydration is necessary to restore moisture to the polymer. We recommend 5 days of continuous exposure to 25C/50% for the HDC3021. If you do not rehydrate the devices after assembly, they may read a negative RH error. We do not recommend baking after assembly.

    3. By sensitivitly, I am assuming you mean RH accuracy. Yes we take the effects of rehydration into account for the datasheet accuracy numbers. 

    4. Rehydration should be done after soldering & assembly. Baking should be done if you observe a positive RH error that makes the device out-of-spec. A 100C 2 hour bake should be sufficient to lower the device's humidity reading by eliminating excess moisture in the polymer.

    Regards

    -Alex Thompson