This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Flash to IWR1443BOOST

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Dear Sir

We received the following response from you, but we would like to confirm the following.

1. Is IWR1443BOOST not needed after flashing once?

2. Is the flash required even when the power is turned off and then turned on again? Or will the flashed demo run if I press the Reset (NRST) button?

3.It says that if I send .cfg, IWR1443BOOST will return the detected data from XDS110 Application /User UART port ,

   but I would like to use the received data without using Visualizer.Is it just a list of detected data?

  What is the format and structure of the data?

4. To run the IWR1443 BOOST Out of Box demo, do I need to flash the xWR14xx_mmw_demo.bin file to IWR1443BOOST?

Your Anser---------------------------

You need to run the Out of Box demo on IWR1443BOOST and send the .cfg file through the UART. .cfg file contains the configuration for the sensor which allows the user to modify as per their application. Once the confuguration is sent, the point cloud detected by IWR1443BOOST is sent out through XDS110 Class Auxiliary Data Port

You need to download and install mmwave_sdk_02_01_00_04

Flash in below binary on the EVM

mmwave_sdk_02_01_00_04\packages\ti\demo\xwr14xx\mmw\xwr14xx_mmw_demo.bin

Switch to Functional mode.

Send the cfg file using the below visualizer. You can view the point cloud plots in the same visualizer .

Thank you

Hiromichi