This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: IWR1443BOOST Flash

Part Number: IWR1443BOOST

Dear Sir

If you connect your PC to the IWR1443BOOST and run the mmWave Demo Visualizer (xWR14xx_mmw_demo.bin is flashed to the IWR1443BOOST), but want to run other receiving programs for the IWR1443BOOST without using the mmWave Demo Visualizer, Is flash necessary?  

In the above, if the IWR1443BOOST flash data is maintained even when the power is turned off, will the program be transferred from the Flash to the SRAM and executed when the IWR1443BOOST is turned on and the Reset (NRST) button is turned on?

Thank you.

Hiromichi