Greetings All,
I am working on MRR repo from toolbox 1.0.1.7 with SDK 3.6 LTS. I tried the initial configuration from the MRR lab and static objects were displayed normally on the MRR GUI visualizer.
Then I mode some modifications to the chirp parameters like (slope, sampling rate, number of samples, number of loops, ...) and lowered SNR from 14 to 13 db.
The expected scene parameters were met successfully but static objects are almost never displayed. What may be the cause of this issue?
- Is there some parameters of CFAR that need to be changed accordingly?
- Should there be a change in the HPF to allow detection of static objects?
- Is there a minimum detectable velocity equation that needs to be taken into consideration?