This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
we found there are 2 different shape in the same tape for LMT87QDCKRQ1, and checked many different DC, no matter 21+, 22+ or 23+ all has this issue, so could you indicate if it's general situation?
Hello, From the photos this appears to be within POD dimensions. I do clearly see pin 1 marker and top side symbol as well. So this is within normal assembly variations. There should be no electrical/thermal impacts either.
Is the customer having any issues with pick and place of the unit onto the board or this is just an AVI anomaly?