This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: LAMBDAOVER2D value in Capon Beamformer steering vector definitions

Part Number: IWR6843AOP


Hi,

 

In radar_toolbox_1_20_00_11\source\ti\dpu\capon3d\modules\DoA\CaponBF2D\src\RADARDEMO_aoaEst2DCaponBF.c at line 162 and 163, when calculating the steering vector values, appears the define LAMBDAOVER2D.

It is defined  at line 67 in radar_toolbox_1_20_00_11\source\ti\dpu\capon3d\modules\DoA\CaponBF2D\src\RADARDEMO_aoaEst2DCaponBF_priv.h as

#define LAMBDAOVER2D (0.9813)

It is not clear to me how it has been derived. Can you explain me the calculations regarding this constant?

 

Thanks,

Riccardo

  • Hello Riccardo,

    Please give us 24 hours to respond with additional information.

    Best Regards,

    Pedrhom

  • Hi,

    LAMBDAOVER2D is the wavelength divided by the distance between two antennas. It should be approximately 1, but due to constraints in design, it is computed to be the value shown above.

    Best,

    nate

  • Hi,

    I've these additional questions:

    1. The spacing between TX antennas in the xWR6843 AoP is equivalent to 1 lambda (half lambda for the RX antennas), which corresponds to 5 mm.  With a speed of light of 3e8 m/s,this is equivalent to a central frequency of 60GHz. Is the value  0.9813 of LAMBDAOVER2D  based on a central frequency different from 60GHz?
      In fact, lambda = 0.9813*2d = 0.9813*5mm = 4.9065mm
       , resulting in a central frequency of 3e8m/s / 4.9065mm = 61.143GHZ
    2. From a formal point of view,  the steering vector formulation provided in Section 6.1.1.1 of the 3D People Tracking Demo Software Implementation Guide – Rev 2.2 suggests that  the correct name should be 2DOVERLAMBDA instead of LAMBDAOVER2D. Is there a typo in the name (but in this case how this number is calculated?) or does it depend on the specific steering vector formulation used in RADARDEMO_aoaEst2DCaponBF_create()?
    3. In the same function, LAMBDAOVER2D is present at lines 162-163 for the azimuth steering vector but it is missing at lines 175-176 for the elevation one. Is there a typo or a mathematical reason for this discrepancy?

    Thanks,

    Riccardo

  • The spacing between TX antennas in the xWR6843 AoP is equivalent to 1 lambda (half lambda for the RX antennas), which corresponds to 5 mm.  With a speed of light of 3e8 m/s,this is equivalent to a central frequency of 60GHz. Is the value  0.9813 of LAMBDAOVER2D  based on a central frequency different from 60GHz?

    You are correct that this will vary as your chirp center frequency changes. I think it's likely this factor came from a specific chirp profile where that was the corresponding center frequency.

    From a formal point of view,  the steering vector formulation provided in Section 6.1.1.1 of the 3D People Tracking Demo Software Implementation Guide – Rev 2.2 suggests that  the correct name should be 2DOVERLAMBDA instead of LAMBDAOVER2D. Is there a typo in the name (but in this case how this number is calculated?) or does it depend on the specific steering vector formulation used in RADARDEMO_aoaEst2DCaponBF_create()?

    What in this document suggests that it should be 2DOVERLAMBDA?

    1. In the same function, LAMBDAOVER2D is present at lines 162-163 for the azimuth steering vector but it is missing at lines 175-176 for the elevation one. Is there a typo or a mathematical reason for this discrepancy?

    Wouldn't the factor of LAMBDAOVER2D be taken care of in the azimuth steering vector? I believe multiplying by the LAMBDAOVER2D factor again would be a double multiplication.

    Best,

    Nate

  • Hi,

    Regarding the answers:

    1. Do you know to which central frequency the value 0.9813 for LAMBDAOVER2D, which is defined at compile time, correspond? Moreover I suspect that using the code with a chirp configuration not aligned with the expected central frequency will produce some degree of error in the resulting heatmap.
    2. The document is 3D_people_tracking_demo_implementation_guide.pdf from radar_toolbox_1_20_00_11, in particular in the section 6.1.1.1 pag 29 we read in which a factor 2DOVERLAMBDA is defined instead of LAMBDAOVER2D
    3. We expected the elevation and azimuth steering vectors to be indipendent, so LAMBDAOVER2D is needed in the elevation one:
     for (i = 0; i < (int32_t)handle->raHeatMap_handle->azimSearchLen; i++ )
    {
    for (j = 0; j < (int32_t)handle->nRxAnt; j++)
    {
    tempfRe = (float)cossp_i(-RADARDEMO_AOAESTBF_PI * LAMBDAOVER2D * moduleConfig->m_ind[j] * currentAngle) * (float) moduleConfig->phaseRot[j];
    tempfIm = (float)sinsp_i(-RADARDEMO_AOAESTBF_PI * LAMBDAOVER2D * moduleConfig->m_ind[j] * currentAngle) * (float) moduleConfig->phaseRot[j];
    _amem8_f2(steerVecPtr++) = _complex_mpysp(_ftof2(tempfRe, tempfIm), _amem8_f2(&moduleConfig->phaseCompVect[j]));
    }
    currentAngle += handle->raHeatMap_handle->nuStep;
    }

    currentAngle = handle->raHeatMap_handle->muInit;
    steerVecPtr = (__float2_t *)handle->raHeatMap_handle->steeringVecElev;
    for (i = 0; i < (int32_t)handle->raHeatMap_handle->elevSearchLen; i++ )
    {
    for (j = 0; j < (int32_t)handle->nRxAnt; j++)
    {
    tempfRe = (float)cossp_i(-RADARDEMO_AOAESTBF_PI * moduleConfig->n_ind[j] * currentAngle);
    tempfIm = (float)sinsp_i(-RADARDEMO_AOAESTBF_PI * moduleConfig->n_ind[j] * currentAngle);
    _amem8_f2(steerVecPtr++) = _ftof2(tempfRe, tempfIm);
    }
    currentAngle += handle->raHeatMap_handle->muStep;
    }

    Thanks,

    Riccardo

    • Do you know to which central frequency the value 0.9813 for LAMBDAOVER2D, which is defined at compile time, correspond? Moreover I suspect that using the code with a chirp configuration not aligned with the expected central frequency will produce some degree of error in the resulting heatmap.

    Yes that appears correct. I would modify this to work with your center frequency.

    For items 2/3, I am investigating now. Please give me a day to come up with a complete answer.

    Best,

    Nate

  • Hi,

    any news?

    Best Regards,

    Riccardo

  • Hi Riccardo,

    You are correct for both. The LAMDBA/2 parameter should be applied for both the azimuth/elevation cases, and it should be 2/LAMBDA as well.

    Best,

    Nate

  • Hi Nathan,
    To ensure complete clarity:
    1- The name LAMBDAOVER2D is incorrect and has to be changed to 2DOVERLAMBDA. But has the numerical value also to be reversed, as it is currently calculated as lambda/(2*D) instead of (2*D)/lambda?
    2- In the radar_toolbox_1_20_00_11, for the elevation case, this parameter is missing and has to be added. Right?
    Thanks,
    Riccardo
  • 1- The name LAMBDAOVER2D is incorrect and has to be changed to 2DOVERLAMBDA. But has the numerical value also to be reversed, as it is currently calculated as lambda/(2*D) instead of (2*D)/lambda?

    No, I think the value is fine. It just corresponds to a specific center frequency. My advice would be to recalculate it based off the center frequency of the chirp you use. In the formula given, you should divide by LAMBDAOVER2D, not multiply by it.

    2- In the radar_toolbox_1_20_00_11, for the elevation case, this parameter is missing and has to be added. Right?

    Yes, It could be added for improved accuracy.

    Best,

    Nate

  • Hi Nathan,

    Thanks for the explanation.

    Riccardo