This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Unable to flash custom board

Part Number: IWR6843AOP
Other Parts Discussed in Thread: UNIFLASH,

Hi,

I'm unable to flash my custom board based on IWR6843AOP using Uniflash and sdk prebuild binary. I'm using RS232_TX, RX (U16, V16) board's pins connected using FTDI cable.   

Uniflash console error:

[30. 10. 2023 18:09:18] [INFO] Cortex_R4_0: Initialization complete.
[30. 10. 2023 18:09:18] [INFO] Cortex_R4_0: Flashing process starting...
[30. 10. 2023 18:09:18] [INFO] Cortex_R4_0: Connecting to COM Port COM6...
[30. 10. 2023 18:09:18] [INFO] Cortex_R4_0: Reset connection to device
[30. 10. 2023 18:09:18] [INFO] Cortex_R4_0: Set break signal
[30. 10. 2023 18:09:38] [ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before re-flashing.
[30. 10. 2023 18:09:38] [ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.
[30. 10. 2023 18:09:38] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[30. 10. 2023 18:09:38] [INFO] Cortex_R4_0: Instance deinitialized!

I also tried to monitor serial communication using oscilloscope seeing break signal, however, no response present. Could you please check my design? Is it possible to provide it not in public way here?

Thank you,

Adam