This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: BPM decoding in HWA is not working

Part Number: AWR2944

Hello,

I'm trying to implement BPM from Tx side and Rx side.

in Tx side i can see that BPM is done as expected, but in Rx side i can see there is no effect.

I can see ADC data with decoding is the same as with no decoding.

I've configured BPM decoding sequence then enabled the BPM mode by setting 1 in "bpmEnable" in fft1d parameter set.

did i miss something that makes the decoding is not working?

Thank you