This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM96000: Junction-to-ambient detail information of LM96000

Part Number: LM96000

Team,

I did not see information about the title in the DS, may anyone can provide it to customer?

Customer need this for the thermal modeling, thanks.

Jeremy.

  • Hi Jeremy,

    The package dissipation spec includes the following footnote on junction-to-ambient thermal resistance: (5) Thermal resistance junction-to-ambient when attached to a double-sided printed circuit board with 1 oz. foil is 113 °C/W.

    Best regards,

    Simon Rojas