Other Parts Discussed in Thread: UNIFLASH, IWR1642, IWR1843, IWR6843
Hi,
I am using a IWR1642BOOST and I am trying to run the Out of the Box demo and when I run it on the mmWave Demo Visualizer nothing happens except for " COM5:115200, COM6:921600 waiting for data ..."
I have followed the initial steps of:
- 1. Setting the Hardware of Flashing Mode SOP0: ON and SOP2: ON
- 2. Toggle the NRST
- 3. Select the CFG_Port COM on UniFlash (COM5 in my case)
- 4. Load the Image from: C:\ti\radar_toolbox_1_30_00_05\source\ti\examples\Out_Of_Box_Demo\prebuilt_binaries
- 5. Setting the Hardware to Funtional Mode SOP0: ON
- 6. Run the Visualizer and select the CFG_Port (COM5) and Data_Port (COM6)
And nothing happens on the console or the graphs and there is only comms when I connect (looked on Wireshark).
And when i send the "Config to mmWave Device" only 2 messages are sent:
Can you help me with this ? Why do I not have any readings ?
Thank you.
Regards.