Part Number: OPT3101-SDK
Other Parts Discussed in Thread: OPT3101EVM, OPT3101
Hi Team,
Using the OPT3101EVM with the MSP430F5529LP hardware, open the INLAB_step_1 condition in the SDK to compile.

The calibration distance parameters are not modified and default is 10mm, 20mm, 80mm, 120mm. After calibration, there is a problem with the output data distance and the threshold can be exceeded and the actual value is significantly different. The customer would like to know is it expected that the measured distance will vary significantly after this step calibration is performed?
The next calibration steps will allow for proper distance measurement. Fixed at 120 mm from the white object, the output data is as follows:

Could you help check this case? Thanks.
Best Regards,
Cherry