This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: Connect the UVC camera via USB on the MMWCAS-DSP-EVM board

Part Number: MMWCAS-DSP-EVM


Hi Team,

The customer is trying to connect the UVC camera via the USB interface that comes with the MMWCAS-DSP-EVM board, currently using the tda2xx_cascade_Linux_radar version configuration. But the system does not react when connecting the camera to the USB3.0 connector on the board.

Could you help share how to modify the profile for UVC camera to be supported? Is it required to install additional drivers or kernel modules? Thanks.

Best Regards,

Cherry