Part Number: OPT3004
Dear Sir/Madam,
I need to connect four OPT3004 in one I2C bus. Based on the table 8-1 on the datasheet, the I2C can be configured in four different ways, connecting to VDD/GND/SCL/SDA.
My question is, how should I connect ADDR to SCL or SDA? Should I use a series 10K resistance or short them directly?


Sincerely
webber