This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL1432BOOST: How to use mmWave Studio

Part Number: AWRL1432BOOST


Hello,

I am trying to get raw data from AWRL1432BOOST using DCA1000.

Board is configured to Debug mode as below table.

And both AWRL1432BOOST and DCA1000 are powered by 5V.

mmWave studio version 2.1.1.0 is used.

<Test step>

1) Reset

2) Connect application/user port (115200 baud rate)

3) Operating frequency :77GHz

    Device variant: XWR14xx(There is no option for XWRL14xx)

4) Load BSS FW: xwr12xx_xwr14xx_radarss.bin

5) Load MSS: xwr12xx_xwr14xx_masterss.bin

 

It works until 4. There is no progress at 5.

Please let me know how can I fix the problem?