This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: I need the source code of IWR6843 for vital sign monitoring

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR6843AOP

I purchased the IWR6843AOPEVM for patient monitoring, the board hasn't arrived but I'm using it to check a vital signs monitoring lab.

The lab states:
"Source code not provided. This lab is provided as a binary file without source code. It can be used to test the application in various use cases. For more information on source code and implementation, please contact your local TI sales representative."

How can I get the source code to evaluate the IWR6843AOP? Or can you provide me with the contact details of a representative at TI Korea for support?

Also, when I look at the menu of mmWave Industrial Visualizer, the demo modes are "Vital Signs with People Tracking", "People Tracking", "Long Range People Detection", etc. Do I need to flash the binary file separately for each of these modes?