Hello,
My client is considering using TMCS1123 to measure current in the energy measurement circuit of an EV charger. The minimal current in the measurement range is 50mA and the needed accuracy of the energy measurement in that range is 2.5% on the room temperature.
I have two concerns regarding this approach:
1. Offset:
Is it possible to calibrate out the offset in the production? Is the offset for a particular sensor same for a given temperature during the lifetime of a device? Additionally, is the temperature drift a constant that can be determined by measuring the offset on two temperatures during the production?
2. Noise:
The stated input noise density is 150uA/sqrt(Hz), as anti-aliasing filter before the ADC has a bandwidth of 7kHz that would mean that the Irms noise is around 12mA, which prevents us from achieving desired precision. Was my calculation correct?
BR
Ugljesa