This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Sensor configuration over CAN

Part Number: IWR6843AOP


Hi,

I am using modified firmware based on the OOB demo. I have made adjustments to replace UART communication with CAN and implemented hard-coded sensor configuration.

For my application, it would be beneficial to configure the sensor via the CAN interface, at least for a portion of the full configuration. Specifically, I plan to operate multiple sensors on a shared CAN bus, and each sensor should have a unique ID for CAN message identification.

If configuring over the CAN interface is not feasible, I may have to compile firmware separately for each sensor, with the only difference being the ID.

Is this possible?

Thank you,

Adam