This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: Resolution testing

Part Number: TMP117


Hello,

I am planning to use TMP117 in one of our application. In the datasheet of TMP117 I saw the resolution of  0.0078°C(1LSB).

I have few questions on the resolution.

1. How do TI tested the resolution of 0.0078°C, is there any test conducted to support this data? For example, Did you Place in TMP117 in temperature controlled chamber and increased temperature from 25°C to 25.008°C and observed 1LSB change

2. How to test the temperature sensor to verity and validation the resolution?

Thanks,

Muni

  • Hi Muni,

    The resolution of the TMP117 is defined by the internal ADC as seen below:

    We do temperature controlled tests for accuracy--as this is defined as a ±0.3 °C device over the full range. However, resolution is defined by the digital code output.

    Best regards,

    Simon Rojas