Other Parts Discussed in Thread: SK-AM68
Hello,
I am trying to get a raw image from DCC tunining tool with TI SK-AM68 EVK.
I believe, I tried all thing according to your guide web page(https://www.ti.com/lit/an/sprad86/sprad86.pdf?ts=1682003811069).
But I can't get a raw image.
Do I need to run any specific application in EVK side?
How can I check connection status between PC and EVK?
Please provide me detail setup information.
Below are what I checked and setup information.
- Logs in Plug-in output of DCC tuning tool
- Successfully read plugin's buffers
Successfully read full uinterface structure from file C:\ti\DCC\bin\IMX219_REF\DC_Subtraction.dat
Successfully restored internal parameter packs
Request to get RAW image from Target : 192.168.0.78
Loaded communication DLL:itCommun.dll
Error in capturing the RAW image
- Successfully read plugin's buffers
- Checked in my side
- Ping between PC which has DCC tool and TI EVK
- Raw data capture by console command
- media-ctl -V '"imx219 4-0010":0 [fmt:SRGGB10_1X10/1920x1080 field:none]'
- gst-launch-1.0 -v v4l2src num-buffers=5 device=/dev/video2 io-mode=dmabuf ! \ video/x-bayer, width=1920, height=1080, framerate=30/1, format=rggb10 ! \ multifilesink location="imx219-image-10bit.raw"
- Setup Information
- EVK : TI SK-AM68
- SDK version : ti-processor-sdk-linux-edgeai-j721s2-evm-09_00_00_08-Linux-x86-Install.bin
- SDK Image : tisdk-edgeai-image-j721s2-evm.wic.xz (Prebuilt EdgeAI Image)
- DCC Tuning tool version : ver 3.1
- Image Sensor : IMX219 Raw sensor(RPiV2)
Thanks,
Jang